AXIS#.IL.FB

Description

This parameter displays the measured actual q-component current reading.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Arms

Range

± Axis peak current (AXIS#.IPEAK )

Default Value

N/A

Data Type

Float

See Also

N/A

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.ILClosed "Instruction list" This is a low-level language and resembles assembly.FB 0x500A 0x1 DINT 1000:1 - RO True
AXIS2.IL.FB 0x510A 0x1 DINT 1000:1 - RO True